Disabling User Account Control - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active

About this task

Note: This procedure is required if you want to use CCT software in Passthru mode from SCT on a Windows 10/11 computer. If you do not perform these steps, Passthru mode does not function. Also, follow this procedure if you need to download resource files for a VND integration into a supervisory engine.

Procedure

  1. In Control Panel, click System and Security > Action Center. The Action Center window appears.
  2. Click Change User Account Control settings. The User Account Control window appears (Figure 1).
    Figure 1. Disabling User Account Control

  3. Move the slider bar to the bottom position called Never notify.
  4. Click OK.
  5. Restart the computer to make the change effective.