Recovery - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

About this task

We recommend that you set RabbitMQ to restart after first, second, and subsequent failures.

To set recovery action:

Procedure

  1. In Control Panel, select Administrative Tools.
  2. Double-click Services.
  3. Right-click RabbitMQ and select Properties. The RabbitMQ Properties dialog box appears.
  4. Click the Recovery Tab and under the First failure, Second failure, and Subsequent failures drop-down list boxes, select Restart the Service.
  5. Click OK.
    Note: At Release 10.0 and later, RabbitMQ replaces MSMQ. See the following table for each release and its queuing technology.
    Table 1. Metasys Release and queuing technology

    Metasys Release

    MSMQ

    RabbitMQ

    Release 9.0 and earlier

    X

    -

    Release 10.0 and Release 10.1

    X

    X

    Release 11.0 and later

    -

    X

1 Both MSMQ and RabbitMQ are in use at Release 10.0 and Release 10.1. 1
2 MSMQ is not used for queuing data at Release 11.0 and later. MSMQ is still enabled at Release 11.0 for legacy support and backward compatibility purposes only.2