The following figure is an example of the connectivity and additional protocols used in a Metasys system that uses Active Directory service. Table 1 describes the protocols used in Figure 1.
Interaction between Callouts |
Protocol |
Communication Direction |
|
---|---|---|---|
1 |
3, 4, 5, 6, 7 |
Unidirectional |
|
1 |
8, 9, 10 |
Unidirectional |
|
1 |
12, 13, 14, 15 |
Kerberos or NTLMv2, DNS, LDAP, NTP, RPC |
Unidirectional |
2 |
3, 4, 5, 6, 7 |
Unidirectional |
|
2 |
8, 9, 10 |
Unidirectional |
|
8, 9, 10 |
12, 13, 14, 15 |
Kerberos or NTLMv2, LDAP, NTP, RPC |
Unidirectional |