Pre-boot Execution Environment (PXE) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active

Network engines (excluding the SNE, SNC, NxE85 and LCS85) implement a PXE client. If your network uses a Pre-boot Execution Environment (PXE) server, exclude the MAC address for these devices from the PXE server. If you do not exclude the MAC addresses, these devices may not start up properly.