Enabling exact or alternate UPN authentication for SCT - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

About this task

Follow the steps below to enable exact or alternate UPN authentication for SCT. This procedure also enables exact or alternate UPN authentication for all Metasys software installed on the SCT computer.

Procedure

  1. On the SCT computer, open Notepad by right-clicking and selecting Run as Administrator. Click Yes if the User Account Control prompt appears.
  2. In Notepad, click File > Open and browse to:

    C:\Program Files (x86)\Johnson Controls\MetasysIII\Tool

    Note: By default, the Metasys software and databases are installed to the C: drive. If you have customized the installation location, specify the location. For example, if you installed on drive E, use E:\.
  3. Right-click on the web.config file. Click Open.
  4. Modify the following key under the <configuration><appSettings> section from false to true:
    <add key="enableOffice365StyleActiveDirectoryAuthentication" value="true"/>
  5. Save and close the web.config file.
  6. Restart the SCT computer.

    For more information on creating users in the Metasys system, refer to Security Administrator System Technical Bulletin (LIT-1201528) .