Auditing - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

The Metasys system offers user action auditing within the system. In other words, the software can trace each action back to the logged in user who performed the action, and list that information in the Audit Viewer. For Active Directory service users, the name recorded is the fully qualified user name (for example, myuser@division.company.com).

Audits are written to a proprietary data store of the Metasys system, which is a SQL Server database on computer/server platforms (Metasys Servers, including ADS/X, OAS, NxE85, and LCS85) and an XML-based file on the other engine platforms. Audits may be viewed using the Audit Viewer in the Site Management Portal UI.