Warning banners - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
The Warning Banner is an optional feature of the Site Management Portal UI. The banner is a specific warning statement that appears every time you launch the SMP UI. To configure this setting, navigate to the Site object of the Site Director and click the Site View tab. In the Warning Banner section, select one of the following, as shown in the following figure below:
  • U.S. Department of Defense (DoD) Warning Banner
  • U.S. General Services Administration (GSA) Warning Banner
  • U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA) Warning Banner
Figure 1. Warning Banner Selection List on Site Object

Once enabled, the Warning Banner you selected appears for all local and Active Directory service users when they log in to the SMP UI of either a Metasys Server or network engine. All local and Active Directory users must agree to the conditions on the warning statement before access is granted.

Notes:
  • After you change the warning banner, the change can take up to five minutes to activate on all network engines that report to the Site Director, because the Site Director needs time to initiate the change to all its child devices.
  • Whenever an operator changes the Warning Banner selection, an entry is sent to the audit log in System Activity for sites using Metasys UI, and the audit log in the Audit Viewer for sites using SMP.
  • The Warning Banner does not appear before you+ log in to the Metasys Advanced Reporting System, SCT UI, Metasys UI, Johnson Controls System Configuration Tool (JCT), or LonWorks® Control Server (LCS85).
  • The only method for removing the Warning Banner from the login process is to set the Warning Banner attribute on the Site object to None. The Warning Banner attribute is stored in the device archive. If you download the Metasys Server from an archive that has been uploaded with the banner option enabled, the banner appears.
Figure 2. Warning Banner entry in System Activity

When the Metasys system login screen appears, you have up to 30 seconds to log in. If 30 seconds passes with no user activity, the login screen closes and the Warning Banner screen returns. The Warning Banner also reappears after you log out of the Metasys system or the system logs you out because of user inactivity.

The Warning Banner remains on the screen until either you click OK, I AGREE, or you manually close the banner window. The banner does not close on its own.

The following figure is a representation of the Warning Banner that appears if you have selected the U.S. Department of Defense (DoD) Warning Banner.

Figure 3. United States DoD Warning Banner

The following figure is a representation of the Warning Banner that appears if you have selected the U.S. General Services Administration (GSA) Warning Banner.

Figure 4. U.S. GSA Warning Banner

The following figure is a representation of the Warning Banner that appears if you have selected the U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA) Warning Banner.

Figure 5. U.S. DOT/FAA Warning Banner