Metasys system architecture - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

Figure 1 shows one example of the many ways you can design the Metasys system architecture.

Note: Restrictions apply to the engines supported with an ADS-Lite Site Director. Refer to the Metasys System Configuration Guide (LIT-12011832) .
Figure 1. Metasys System Architecture