Metasys dial-up networking - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

Point-to-Point (PPP) networking is used for all dial-up communication between the Metasys client computer (web browser) and the Metasys server and engine. Newer models of network engines and the latest release of Metasys Server software do not support communication over modems. If you have an older system, refer to the Metasys System Extended Architecture Direct Connection and Dial-Up Connection Application Note (LIT-1201639) for more information.