Appendix: Windows Desktop OS considerations - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

This appendix covers important considerations regarding the use of Metasys system software on Windows desktop operating systems.

Release 13.0 of the Metasys system supports the following operating systems: Windows® 11 Pro and Windows® 11 Enterprise versions 22H2, 21H2 (64-bit), Windows 10 Pro and Windows 10 Enterprise Editions (version 2004, 21H1, 21H2) (64-bit), Windows 10 Enterprise LTSC (21H2), Windows Server 2022, and Windows Server 2019 (version 1809 or later) (64-bit).

These Windows desktop operating systems offer increased network security that affects Internet and intranet communication, including communication between Metasys system components.

For information on firewall settings required for Metasys system communication, see Appendix: Windows firewall.