Trap format - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

When an object with an alarm extension generates an event in the Metasys system, the SNMP service sends a trap to the NMS. No matter what type of event occurs, the Trap OID sends out the same set of attributes. Table 1 lists the attributes.