Field device disable/enable - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active

When the user or a process disables communication to a field device, the SNMP Agent sends a trap regarding the Disable command in a similar manner as the Alarm Raised trap. The eventValue indicates Comm Disabled.

When a Comm Enabled command to the device occurs, the SNMP Agent sends a trap regarding the Enable command as well as a separate alarm trap regarding the return to online status.