Translating attribute values - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English
As highlighted in the Trap Examples section, each Trap OID sends the same set of attributes. You can translate attributes values (evPreviousState) using the key values in the following table.
Table 1. Device Diagnostic Attributes

Key

Text

Key

Text

0

Normal

68

Alarm

1

Fault

69

Trouble

2

Off Normal

70

Status

3

High Limit

71

Offline

4

Low Limit

72

Shutdown

64

Low Warning

73

Unreliable

65

High Warning

75

Online

66

Low Alarm

65535

Unknown Previous State

67

High Alarm