Base OID - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

1.3.6.1.4.1.4399.2.1.1.1.1.4.1.1.x.y

where x is an integer that represents the attribute of the point and y is an ASCII representation for the name of the Metasys point (Table 1).