Get request base OID - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

The Base OID for any Get Request is as follows:

1.3.6.1.4.1.4399.2.1.1.1.1.4.1.1.x.y

where x is an integer that represents the attribute of the point (Table 1) and y is an ASCII representation for the name of the Metasys point.

Table 1. Point Attributes

x

Description

.85

Present Value

.103

Reliability

.117

Units

.661

Display Precision

.1006

Alarm State

.32527

Item Reference

The two primary Get Requests are the Point Attribute Get Request and the Device Diagnostics Get Request.