Alarm raised trap - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

When an object with an alarm extension generates an event in the Metasys system, the SNMP Agent sends the same Alarm Type that was raised in the system (Metasys Server or network engine). Examples include High Warning and Low Alarm. Each Trap OID also sends the attribute values that were selected for the trap (Table 1).