Dynamic Host Configuration Protocol (DHCP) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

A communications protocol that lets network administrators centrally manage and automate the assignment of IP addresses in an organization’s network.

DHCP lets a network administrator supervise and distribute IP addresses from a central point and automatically sends a new IP address when a device is plugged into a different location on the network. DHCP can also assign dial-up users an IP address automatically when they connect to the network. Some DHCP servers can support fixed addresses for devices that need a static IP address.

The Metasys server, network engine, TEC20 Coordinator, and Many-to-One Wireless Room Temperature Sensing Receiver (WRS-RTN) can obtain their IP addresses and other network information using DHCP. Each Metasys device that can connect to the Ethernet network needs a unique IP address. Without DHCP, the IP address must be entered manually for each device; and, if the devices are moved to another subnet on the network, you must enter a new IP address. The Metasys system supports both dynamic and static IP address assignments.