Domain Name System (DNS) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active

The method by which host domain names are translated into IP addresses. A domain name is a meaningful and easy-to-remember handle for an Internet address. DNS is the Internet standard for naming host devices and mapping host names to IP addresses.