Demilitarized Zone (DMZ) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active

A portion of the network located between the Internet and the intranet. It is a buffered area that is usually protected by two or more firewalls.