The formal definition of all object and attribute data that can be stored in the directory; for example, user is an object type with attribute data of name, first name, last name, email, and so on. The schema is made up of object classes and attributes. The base (or default) schema contains a rich set of object classes and attributes to meet the needs of most organizations, and is modeled after the ISO X.500 standard for services.