Active Directory Service - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

A network operating technology that enables IT administrators to manage enterprise-wide information from a central repository. This information includes data center policy compliance and identity management (user login accounts), which are used for both Microsoft Windows authentication (login to the Windows operating system) as well as network resource authentication (login to enterprise-wide secured applications, such as email). The Metasys system uses the LDAP integration of Active Directory.