Appendix: Installing antivirus software - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

To install antivirus software on computers that run Metasys software, complete the steps in this appendix. Use one of the following antivirus software programs:

  • Symantec® Endpoint Protection software Corporate Edition version 12.x or later.
  • McAfee® VirusScan® Enterprise version 8.8 with Patch 9 or later.
  • Windows® Defender Antivirus® built into Windows® 11, Windows® 10, Windows® Server® 2022, and Windows® Server® 2019.