SCT computer - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

The computer with the SCT software must be joined to an Active Directory service domain (or trusted domain) where the Metasys system users are located.

In addition, configure any firewalls to allow appropriate Active Directory service communication.