Metasys server computer - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

The computer with the Metasys server software (ADS, ADX, MVE, or OAS) must be:

  • joined to an Active Directory service domain (or trusted domain) where the Metasys system users are located

  • added to an Active Directory service domain where the computer is not affected by group policies

In addition, configure any firewalls to allow appropriate Active Directory service communication.