Appendix: Active Directory service - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0

Network and IT Guidance Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

This appendix provides additional information to network managers for configuring the Active Directory service for use with the Metasys system on a computer that has the Metasys server or SCT software installed.