Refer to the literature for the Metasys products you are installing for a list of supported operating system and SQL Server software versions. For an overview of software supported by the Metasys system, refer to the Metasys Server Installation and Upgrade Instructions (LIT-12012162) , SCT Installation and Upgrade Instructions (LIT-12012067) , or the Open Application Server Installation and Upgrade Instructions (LIT-12013222) .
As new software and service packs become available, Johnson Controls tests them for use with Metasys software. Be aware that installing other software or updating the operating system with a new service pack on a computer running Metasys software may adversely affect the system.
The following table lists the versions of IIS that can be used with Metasys products.
|
Operating System |
Supported IIS Version |
|---|---|
|
IIS 10.0 |