Turning off the Internet Explorer Web Browser pop-up blocker - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

This procedure applies to the Internet Explorer pop-up blocker. If you have third-party pop-up blockers, use the manufacturer’s instructions to disable them.

To turn off the pop-up blocker:

  1. Open Internet Explorer.
  2. On the Tools menu, select Pop-up Blocker > Turn Off Pop-up Blocker.
Note: For information on allowing pop-ups from specific sites only, refer to the Internet Explorer Help.