Support for Active Directory/LDAP service (including single sign-on capability) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Table 1 is a summary of which Metasys system application User Interfaces support Active Directory logins and the SSO capability. If the application supports Active Directory logins, then the Metasys system can be configured to use your existing IT Active Directory Service infrastructure for authentication purposes. If the application supports SSO, then you can log in to multiple, secured applications without reentering the same user name and password.

Table 1. Products that support Active Directory/LDAP logins and SSO

Application

Active Directory login supported

Exact or alternate UPN format logins supported

SSO supported

ADS/ADX/OAS Site Management Portal UI

Yes

Yes

Yes

SCT

Yes

Yes

Yes

Metasys UI and Johnson Controls System Configuration Tool (JCT)

Yes

Yes

No

Metasys Advanced Reporting System

No

No

No

Network Engine

No

No

No

Metasys for Validated Environments

Yes

Yes

No

For more details on Active Directory and SSO interaction with Metasys system security, refer to the Security Administrator System Technical Bulletin (LIT-1201528).

1 If you are using Metasys Advanced Reporting System UI on an ADX, you can still use the SSO capability to log in to the ADX Site Management Portal UI. For example, if you have an ADX with the Metasys Advanced Reporting System, you can use SSO to log in to the ADX Site Management Portal UI, but you must enter your Metasys system user name and password pair to log in to the reporting system.
2 The engine Site Management Portal UI does not support authentication with Active Directory service. If you have an ADS/ADX/OAS Site Director, however, you can log in to the ADS/ADX/OAS Site Management Portal UI using SSO and access system information for the entire site, including details on the engine.