Child device considerations - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Child devices, which include network engines, do not use the Active Directory service; however, if the user logs in to a Site Director with Active Directory service credentials, they may navigate to child devices. The child devices:

  • can be any combination of platforms illustrated in Figure 1

  • do not need to be at the same release as the Site Director

  • do not need to join an Active Directory service domain