Users - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The Metasys system has two types of users: local users and Active Directory service users. A local user is defined in the Security Administrator system and is authenticated and authorized against the Metasys Security database. An Active Directory service user is created and stored in an Active Directory service domain and is added as a Metasys system user with the Security Administrator System. This user is authenticated against an Active Directory service domain and authorized against the Metasys system.

Once logged in, the user is limited to actions that are permitted by the user’s assigned privileges. Refer to the Security Administrator System Technical Bulletin (LIT-1201528) for specific details on Metasys system access security.