Metasys Application Programming Interface (API) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Additional enhancements to the Metasys Server software at Release 10.1 and later include a REST-compliant Metasys Monitoring and Commanding Application Programming Interface (API) that enables reading, writing, and commanding of one or more Metasys objects/properties to provide a secure way to bi-directionally integrate with third-party applications. As a prerequisite, you need to define a new user of type API Access under the Security Administrator system of the Site Management Portal that provides access to the Metasys system. For details, refer to the Security Administrator System Technical Bulletin (LIT-1201528).

This is the latest in a suite of APIs that include the REST-compliant API that enables data to be securely extracted from the Metasys system and integrated with third-party data visualization tools to meet robust data analysis and reporting needs and the Metasys API for the TeleHealth Engagement Application that facilitates reliable two-way communication between the TeleHealth patient engagement application and Metasys system to provide patients direct control over their healthcare space for increased comfort and satisfaction.