Field bus considerations - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Metasys system devices that connect to Ethernet networks use various field buses to interface with the building control system. Field buses provide direct connections between field devices and the supervisory device that controls them. Possible field buses include the LonWorks network, MS/TP bus, and N2 Bus. For information on the buses supported by specific Metasys system devices, refer to the product literature for each device.