Database management: SQL Server tools - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

In addition to or instead of the Metasys Database Manager, you can use the following Microsoft Corporation tools to maintain your SQL Server databases:

Table 1. SQL Server Software Maintenance Tools

SQL Server Software Family

Microsoft Corporation Database Tool

Included with SQL Server Software?

SQL Server Software

SQL Server Management Studio

Yes

SQL Server Express Software

Microsoft SQL Server Management Studio Express (SSMSE)

No

For specific steps on how to back up and manage Metasys system databases using these tools, go to http://www.microsoft.com. You do not need to stop Metasys system services to perform a database backup.

1 All tools are available on http://www.microsoft.com/downloads.
2 Available with versions that include Management Tools or Advanced Services.