Database management: Metasys Database Manager - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The Metasys Database Manager allows you to purge, back up, restore, and monitor your Metasys system SQL Server databases. This tool is included on all Metasys server media and is compatible with all versions of SQL Server software supported by the installed release of Metasys software. Refer to the Metasys Database Manager Help (LIT-12011202) for more information.