BACnet/SC - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

BACnet Secure Connect (BACnet/SC) is a new BACnet datalink, ASHRAE 135-2020 Annex AB, that provides secure message transport by using the standard IP application protocol, Secure WebSocket, which is an extension to HTTPS and runs over Transport Layer Security (TLS). BACnet/SC thereby provides a secure mechanism to authenticate and authorize a device to use the network. From a cybersecurity standpoint, mixing BACnet/IP and BACnet/SC compromises the security of the network. It is best practice to use only BACnet/SC for the entire site to safeguard a site's security, if possible. If you must connect BACnet/IP devices, it is best practice to minimize the number of BACnet/IP devices and isolate them to one engine.