Summary of changes - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The following information is new or revised at release 13.0.50:

  • Removed Pre-boot Execution Environment (PXE) sections as it is no longer supported.
  • Updated Metasys for Validated Environments (MVE) to reflect updated OS and SQL Server requirements at Release 13.0.50.