Windows features not supported by Metasys software - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Metasys software does not support the following Windows features:

  • Sleep. If you install a Metasys server or SCT on Windows 10 or Windows 11, you must turn off the Sleep feature. Failure to turn off this feature can result in communication problems when the Metasys server or SCT goes to sleep.

  • Fast User Switching. Users must log off instead of switching users.