Administrator rights - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Administrative privileges may function differently on Windows 11 and Windows 10. Depending on your operating system login privileges, you may need to perform additional steps to use Metasys software (including logs) or access Windows operating system features and SQL Server software.

Table 1. Login Privileges and Steps

Login Privileges

Steps to Run Software

Not logged in as the Windows account named Administrator

To run the software when the Windows operating system is using the standard interface:
  1. Right-click the application icon on your desktop or software name in a menu.
  2. Select Run As Administrator or More > Run As Administrator.
  3. If prompted, enter your credentials.
  4. Click Yes.
To run the software when the Windows operating system is using the Tile interface:
  1. Right-click the application tile on the Start screen.
  2. Select Run As Administrator on the bottom of the screen.
  3. If prompted, enter your credentials.
  4. Click Yes.

Refer to the documentation for the specific Metasys software you are using for more information on how to perform tasks that require Administrator privileges.

Logged in as the Windows account named Administrator

Run the software without additional steps.