Example - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The difference between the SNMP Trap generated for a binary point that goes into Alarm and one whose status transitions to Return to Normal is outlined in the following table.

Table 1. SNMP Trap Attribute Example

SNMP Trap Attribute

Alarm Value

Normal Value

snmpTRAPOID.O

alarmEvent

normalEvent

EventValue

Active

Inactive

EventPreviousStatus

0

68

EventMessage

Alarm message defined in the Metasys Site Management Portal UI

Return to Normal message defined in Metasys Site Management Portal UI