The Base OID for any Get Request is as follows:
1.3.6.1.4.1.4399.2.1.1.1.1.4.1.1.x.y
where x is an integer that represents the attribute of the point (Table 1) and y is an ASCII representation for the name of the Metasys point.
|
x |
Description |
|---|---|
|
.85 |
Present Value |
|
.103 |
Reliability |
|
.117 |
Units |
|
.661 |
Display Precision |
|
.1006 |
Alarm State |
|
.32527 |
Item Reference |
The two primary Get Requests are the Point Attribute Get Request and the Device Diagnostics Get Request.