SNMP Get requests - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

SNMP Get requests allow the NMS to request information for a specific variable. The SNMP agent, upon receiving a Get message, issues a GET-RESPONSE message to the NMS with either the information requested or an error indication as to why the request cannot be processed.

The Metasys SNMP Agent allows you to perform SNMP Gets on pre-defined OIDs of certain objects (for example, Analog Value [AV], Binary Value [BV], and Multistate Value [MV] objects). For a list of the attributes that are available for polling, see Table 1.

Note: To use Gets, you must query the specific supervisory device (SNE22 for example) on which the object appears. Site Directors do not forward Get requests to other devices on the site and you cannot perform Gets on ADSs/ADXs.

The Metasys SNMP Agent also allows you to determine the health of the device by polling the OIDs listed under Table 1. These attributes include data such as battery condition and object count.

You can poll all the points on the network engine, but there is a limit on SNMP Gets, which is two requests per second. For example, polling 500 points on a single engine takes about five minutes.