Of the available attributes listed in Table 1, configure the NMS interface to filter the attributes to be trapped. You also must select these attributes when you configure the SNMP DDA alarm notifications and destinations in the device object. For details, refer to the SNE Commissioning Guide (LIT-12013352), SNC Commissioning Guide (LIT-12013295), Open Application Server (OAS) Commissioning Guide (LIT-12013243), and the ADS/ADX Commissioning Guide (LIT-1201645). This list applies to Metasys alarm events only.
|
Field Names |
||
|---|---|---|
|
ackRequired |
eventValue |
itemName |
|
eventDetectionTimestamp |
evPriority |
SiteName |
|
eventMessage |
itemCategory |
units |
|
eventPreviousStatus |
itemDescription |
|
|
eventUniqueIdentifier |
itemFullyQualifiedReference |
|