Alarm synchronization - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The Metasys SNMP Agent does not support Alarm Synchronization, a function that indicates to the NMS which Metasys objects went into alarm while the NMS was offline. The SNMP Agent assumes that the NMS received the alarm and, therefore, does not rebroadcast it. Even though alarm synchronization is not performed, the SNMP Agent allows the NMS to poll points and device attributes to determine their statuses. From this information, the NMS can determine which points are reporting Alarms and react accordingly.