Metasys SNMP MIB files - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Three Johnson Controls® MIB files are provided on the product media and on the Metasys system website for download https://my.jci.com/sites/BE/NABAS/Pages/Metasys_System_Extended_Architecture/Metasys_System_Extended_Architecture_Deployment/deployment/5_2_MIB.aspx (Table 1). The NMS software can read these MIB files, as well as the standard MIB files.

Table 1. List of Johnson Controls and Standard MIB Files

Johnson Controls MIB Files

Standard MIB Files 1

 

jcicontrolsgroup.mi2

SNMPV2_MIB.mib

 

johnsoncontrolsinc.mi2

SNMPV2_SMI.mib

msea.mi2

SNMPV2_TC.mib

These MIB files define the data available from the Metasys SNMP feature. They provide the OIDs that describe the traps and point types available in the Metasys system. For example, an OID is available to describe the alarm state of a point. Loading the MIB files into the NMS provides translation of the Metasys data.

1 Standard MIB files are available on the Internet.