Limitations - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

The following are the limitations of NMS and Metasys SNMP agent functionality:

  • NMS does not provide the ability to acknowledge and/or discard Alarms by using an SNMP Set message.

  • NMS cannot modify the supervisory device by using an SNMP Set message.

  • Metasys SNMP Agent functionality does not allow the NMS to detect when the supervisory device suffers a power failure or to initiate any action based on such detection.

  • SNMP Get requests are not proxied through the site; that is, you must query the device of interest directly and not through the Site Director.

  • With the SNMP Version 3 implementation, user authentication, and data encryption are not available for SNMP traps and Gets.

  • The Get Bulk request, which returns data from multiple objects with one request, is not supported.