User Datagram Protocol (UDP) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

A communications protocol that offers a limited amount of service when messages are exchanged between computers in a network that uses IP. User Datagram Protocol (UDP) is an alternative to TCP. Like TCP, UDP uses the Internet Protocol to actually get a data unit (called a datagram) from one computer to another. Unlike TCP, UDP does not divide a message into packets (datagrams) and reassemble it at the other end. Specifically, UDP does not provide sequencing of the packets that the data arrives in; therefore, the application program that uses UDP must ensure that the entire message has arrived and is in the right order.