Transport Layer Security (TLS) and Secure Sockets Layer (SSL) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Transport Layer Security (TLS) is the successor to the Secure Sockets Layer (SSL) protocol. Both communication protocols provide network security to client-server applications.

For general information on how to implement TLS or SSL, refer to https://technet.microsoft.com/en-us/library/cc784450(v=ws.10).aspx.

The Metasys software can use Secure Channel and built-in implementation of TLS or SSL included with the Microsoft Windows operating system. For more information about Secure Channel, refer to https://msdn.microsoft.com/en-us/library/windows/desktop/aa380123(v=vs.85).aspx.