Simple Network Time Protocol (SNTP) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

A simplified version of NTP. These protocols allow one computer to ask another computer for the time across a TCP/IP network, then set its own clock accordingly. A number of public Simple Network Time Protocol (SNTP) time servers keep track of time with a very high degree of accuracy that can be used to ensure that the Site Director is synced to real time.