Point-to-Point Protocol (PPP) - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

A protocol for communication between two computers using a serial interface, typically a computer connected by phone line to a server. It is sometimes considered a member of the TCP/IP suite of protocols. Relative to the OSI reference model, PPP provides layer 2 (data-link layer) service.