Licensing requirements overview for operating systems - Metasys - LIT-12011279 - General System Information - Metasys System - 13.0.50

Network and IT Guidance Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011279
Version
13.0.50
Revision date
2024-01-26
Product status
Active

Windows operating system license requirements

The Microsoft Server operating system software used by the ADS/ADX requires licenses called Client Access Licenses (CALs). A CAL is a license that gives you the right to access the services of the server. Two types of Microsoft operating system CALs are available: a device-based CAL and a user-based CAL. You need to purchase the CALs separately from the ADX server.

For more information on CALs, refer to https://www.microsoft.com/en-us/licensing/product-licensing/client-access-license.